{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Java Cryptography Extension requirement for connecting to Nutanix Cluster in PowerChute Network Shutdown
Issue:
It is necessary to install the Java Cryptography Extension policy files in specific geographies to connect to a Nutanix Cluster that requires a 256-bit cipher.

Product:
PowerChute Network Shutdown v4.3

Environment:
All supported operating systems

Solution:

NOTE: This issue is resolved starting with PowerChute Network Shutdown v4.4, which uses OpenJDK 14.

If installing PowerChute Network Shutdown 4.3 due to the import control restrictions of some countries, the version of the Java Cryptography Extension (JCE) policy files that are bundled with the Java Runtime Environment 8 (JRE 8) allow ‘strong’ but limited cryptography to be used: they have in-built restrictions on available cryptographic strength. Depending on your geographical location (e.g., outside of the United States), to connect to a Nutanix Cluster that requires a 256-bit cipher, it may be necessary first to download and install the Unlimited Strength JavaTM Cryptography Extension (JCE) Policy Files available from the Oracle website.

NOTE: You should consult your export/import control or legal counsel to determine the exact cryptographic strength required for your geographical jurisdiction.

Steps to install the JCE policy files:

  1. Download and extract the Unlimited Strength Jurisdiction Files on the Oracle website.
  2. Navigate to the installed directory of PowerChute Network Shutdown. If the default location were chosen during installation, this would be C:\Program Files (x86)\APC\PowerChute or C:\Program Files\APC\PowerChute, depending on your operating system.
  3. Navigate to \<jre>\lib\security and replace the existing Policy Files with the ones extracted in Step 1.
    • This folder will be named jre_x64 or jre_x86, depending on your operating system.
  4. Restart the PowerChute Network Shutdown service.

Schneider Electric Algeria

En savoir plus
Gamme :
Catégorie :
Les articles qui pourraient être utiles
En savoir plus
Gamme :
Catégorie :