{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Can the AR9000RAMP be used on the shock pallet of the AR3xxxSP cabinets?
Issue:
A customer may want a reusable ramp to use on AR3xxxSP cabinets.

Product Line:
NetShelter SX SP, SX3K

Environment:
All versions and serial ranges.

Cause:
If a customer looses their shock packaging ramp, or requests a reusable ramp, is there one available for the AR3xxxSP cabinets?

Resolution:

The NetShelter shock packaging (AR3xxxSP) cabinets ship with single use wooden ramps.
The NetShelter SX3K Integrator Ready (AR9xxx) cabinets have a reusable metal ramp available with with the cabinet, or separately under sku AR9000RAMP.
The AR9000RAMP is also compatible with the NetShelter SX shock packaging cabinets (AR3xxxSP)

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :