{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Can the ends of a NetShelter 2-post or 4-post rack be closed with panels?
Issue:
The customer wants to close off the ends of their open rack for a clean look.

Product Line:
NetShelter 2-Post and 4-Post racks

Environment:
All versions and serial ranges.

Cause:
The ends of the racks is open, and the equipment and cables are visible.

Resolution:

For customers with 2-post or 4-post racks there is a way to close off the ends for a cleaner look.
Adding Performance Cable Managers to the posts and using the blanking plates creates a solid black endplate. On a 4-post rack it creates the look of a cabinet, instead of an open rack.
For additional information and part numbers please use this link to the NetShelter Cable Management brochure and see the section on Performance Cable Management, pages 19-22: https://www.apc.com/salestools/JCOS-7H4M68/JCOS-7H4M68_R9_EN.pdf
Or, if the 4-post rack has not been purchased you can install a NetShelter SX cabinet that has side panels but no doors, like AR3100X610.


Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :