{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What is the IP (ingress or international protection) rating of SMC, SMT and SMX series Smart-UPS?
Issue:
Ingress or international protection (IP) rating is required for SMC, SMT or SMX series Smart-UPS.

Product Line:
Smart-UPS model numbers beginning with SMC, SMT or SMX only
Note: Other models of Smart-UPS or Back-UPS may meet these same levels of IP, but have not been tested and verified for compliance

Cause:
IP ratings are used to determine how large an object, or liquid, may pass through the side panels, or roof, of an enclosure.

Resolution:
SMC, SMT and SMX models have been tested and verified for compliance with UL/CSA/IEC 60950-1 and are specified with IP rating 20: protects against solid objects greater than 12 mm and does not offer protection against water.

The IP Rating Scale is defined as follows:

1st number of the rating can change from 0-6 and indicates the degree of protection with respect to persons and solid objects.

0 = Not protected
1 = Protects against solid objects greater than 50 mm
2 = Protects against solid objects greater than 12 mm
3 = Protects against solid objects greater than 2.5 mm
4 = Protects against solid objects greater than 1.0 mm
5 = Dust protected
6 = Dust tight

2nd number of the rating can range from 0-8 and indicates degree of protection with respect to harmful ingress of water.

0 = Not protected
1 = Protects against dripping water
2 = Protects against dripping water of +- 15 degree angle
3 = Protects against spraying water of +- 60 degree angle
4 = Protects against splashing water
5 = Protects against water jets
6 = Protected against heavy seas
7 = Protects against immersion
8 = Protects against submersion

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :