{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What is the IP or NEMA rating of the SmartBunker FX?
Issue:
NEMA or IP rating has been requested.

Product Line:
SmartBunker FX

Environment:
All versions and serial ranges.

Cause:
There is no IP or NEMA rating listed in the Technical Specifications.

Resolution:


The SmartBunker FX is not IP/NEMA rated.

The current design of the enclosure does not provide an official dust or water rating. The only statement we can use is that there is an enhancement kit of the gaskets that can prevent vertical leakage from water sprinklers to enter the enclosure.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :