{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What size are the cable ports on the NetShelter CX, and how many are there?
Issue:
Cables need to enter and exit the cabinet.

Product Line:
NetShelter CX2

Environment:
All versions and serial ranges.

Cause:
Knowing the dimension of the cable port allows a person to calculate how many cables can fit through the opening.

Resolution:

AR4000MV: two ports, 30mm x 95mm at the botton and 26mm x 68mm at the top.

AR4018A/AR4018IA: one port, 350mm x 120mm at the bottom.

AR4024A/AR4024IA: one port, 350mm x 120mm at the bottom.
AR4038A/AR4038IA: two ports, 350mm x 120mm, one at the top and one at the bottom.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :