{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Can a 3rd party UPS be installed in the AR106V or AR106VI?
Issue:
It is unknown if a 3rd Party UPS can be installed into the AR106V and AR106VI.


Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The NetShelter WX 6U Vertical cabinets have a mounting bracket for a 2U UPS.

Resolution:

Any 3rd party UPS must be validated by the manufacturer to work with this cabinet prior to installation:
The manufacturer must validate that the 3rd party UPS can be installed vertically. Not all batteries can install in this orientation.
When shipping with a 3rd party UPS installed, the manufacturer must validate that the 3rd party UPS can ship installed using their rail kit(s), without disconnecting in transit.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :