Consulter notre FAQ
Lighting calculation for Lighting Kit part numbers; ACDC2018, ACDC2019
Can Schneider Electric provide lighting calculation files (.ies)? The customer is trying figure out a way to show adherence to our standards with the lighting used in the containment units. We have to have a minimum of 50 foot candles at all racks/cabinets.
Schneider-Electric does not provide such .ies files, however attached is the photometric specs needed. The document gives the footcandles at various locations. Note that if frosted lens are used, a .75 multiplier must be applied. There are qty 4 in the ACDC2018, qty 6 in the ACDC2019
Schneider-Electric does not provide such .ies files, however attached is the photometric specs needed. The document gives the footcandles at various locations. Note that if frosted lens are used, a .75 multiplier must be applied. There are qty 4 in the ACDC2018, qty 6 in the ACDC2019
Publié pour:Schneider Electric Algeria
Pièce(s) jointe(s)
En savoir plus
Produit :
Gamme :
En savoir plus
Produit :
Gamme :