{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
PowerChute Network Shutdown – some VMs are not started for HyperFlex cluster
Issue:
PowerChute Network Shutdown – some VMs are not started for HyperFlex cluster

Products:
PowerChute Network Shutdown v4.4, v4.4.1

Environment:
PowerChute Network Shutdown configured with HyperFlex support with VMware as hypervisor

Cause:
After the HyperFlex cluster service has started, some VMs may still be in an inaccessible state when PowerChute attempts to power them on. When this happens, the power on attempt will be unsuccessful and these VMs are not re-attempted.

Solution:
Increase the Cluster Startup Duration in PowerChute to allow enough time for all VMs to become accessible in the inventory before VM start up occurs.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :