{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Netbotz 750/755 | Using Special Characters for Root and Superuser Password
Netbotz 750/755 | Using Special Characters for Root and Superuser Password

Product Line:
Netbotz 5.x

Environment:
NBRK0750, NBWL0755, potentially any firmware

Cause:
While most special characters for the root and superuser password are supported, including % or + in your passwordwill lock you out.
When the password has any of the 2 unsupported special characters, the appliance will accept the password without any error message. However, logging in with the password will prompt an error that the username or password is incorrect.

Resolution:
These special characters !@#$^&*<>?-=./”()|are accepted by the appliance.  Any combination of these characters should work.
If your root or superuser password includes % or +, follow the password reset procedure below.

NetBotz 750 | Resetting a Lost Root Account Password
NetBotz 700 | Resetting a Lost Super User (Web UI) Account Password

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :