{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.

Consulter notre FAQ

What is the POE specification for the NetBotz 755?

Issue:
What is the POE spec for the NetBotz 755

Product Line:
NBWL0755

Environment:
NetBotz power over ethernet

Cause:
NetBotz 755 requires POE. Not all POE power options are compatible

Resolution:
The NB755 meets the standard for IEEE802.3at and it has a classification resistance of 63 Ohms.
This makes it type 2 device.
A type 3 power supply can also power a type 2 device with no issues.

APC has offered 2 POE injectors:
NBAC0303NA

Power over ethernet PoE up to 18 Watts Supported Products
NBWL0356A
NBWL0456A
EGX150POE

NBAC0303NA2
Power over ethernet PoE+ up to 36 Watts
NBWL0756
IEEE802.3at class 4
(new) (more power)
Also known as Type 2 PoE

Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :