{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Easy UPS Line Interactive: Clicking AVR
If the Easy UPS Line Interactive is frequently on AVR when the input power is stable we recommend, changing the default input voltage. This can be done through the UPSCAPO software v3.2.6 or later.

In the software, select Voltage Setting in the UPS Settings tab.
Voltage Selection

Select Yes in the popup box. Warning: The software and UPS will turn off. Please ensure there is no load connected.
Voltage Selection 2

Select the desired Output Voltage. The options are 220v, 230v or 240v.
Voltage Selection 3

Close the software to save the voltage setting. Restart the software to start managing the software once again.
Voltage Selection 4

Once this has been completed the UPS should no longer go on AVR, when the input power is stable.

Schneider Electric Algeria

Pièce(s) jointe(s)
3.2.6 Setup.zip [4.9 MB]
UPSCAPO user manual-V3.2.6 (English).pdf [1.53 MB]
En savoir plus
Produit :
Les articles qui pourraient être utiles
En savoir plus
Produit :