{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What is the Short Circuit Current Rating of my Smart-UPS On-Line?
Issue: What is the Short Circuit Current Rating of my Smart-UPS On-Line?

Product Line: Smart-UPS On-Line models with the prefixes SRT, SRTL, SURT and SURTD.

Resolution: The short circuit current rating of a Smart-UPS On-Line is typically determined by the UPS input circuit breaker. SRT and SRTL UPS models 1-1.5kVA, and SURT UPS models 1-2kVA feature built-in input circuit breakers rated at 1kA at 250VAC and 2kA at 125VAC,

SRT, SRTL, SURT and SURTD UPS models rated 3kVA and above do not have a built-in input circuit breaker, and it is recommended to install a circuit breaker upstream the input branch of the UPS. The recommended circuit breaker specifications are available in the Installation Manuals of the various Smart-UPS models. The short circuit current rating of the UPS system will be determined by the external input circuit breaker installed upstream the input branch of the UPS.

Note: Although the UPS output short circuit rating is a different specification than the short circuit current rating, customers may wish to know the output short circuit rating of the UPS. The output short circuit of Smart-UPS On-Line models is rated at 175% of nominal output current for up to 500 milliseconds.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :