Issue:
DCE shows duplicate cameras for a single NetBotz 750/755
Product Line:
Data Center Expert
NetBotz
Environment:
DCE (any version)
NBRK0750
NBWL0755
NBPD0165
Cause:
If you Remove a NetBotz 750 or 755 from DCE and that appliance had a connected camera, the camera will not get deleted from DCE surveillance.
The camera will appear as disconnected and show a test pattern. Re-adding the appliance even with the same camera re-adds the camera with a separate internal ID so DCE won't associate it with the newly added NetBotz.
Resolution:
After removing a NetBotz 750 or 755 with a connected camera from DCE, it is recommended that you delete the camera from the surveillance view in DCE.
If you do not, after you re-add the NetBotz even with the same camera, that camera will show as a duplicate and only one camera will actually capure clips going forward.
You should still be able to delete the camera after re-adding the appliance as you will see one communicating and one not communicating. Delete the non-communicating camera.
DCE shows duplicate cameras for a single NetBotz 750/755
Product Line:
Data Center Expert
NetBotz
Environment:
DCE (any version)
NBRK0750
NBWL0755
NBPD0165
Cause:
If you Remove a NetBotz 750 or 755 from DCE and that appliance had a connected camera, the camera will not get deleted from DCE surveillance.
The camera will appear as disconnected and show a test pattern. Re-adding the appliance even with the same camera re-adds the camera with a separate internal ID so DCE won't associate it with the newly added NetBotz.
Resolution:
After removing a NetBotz 750 or 755 with a connected camera from DCE, it is recommended that you delete the camera from the surveillance view in DCE.
If you do not, after you re-add the NetBotz even with the same camera, that camera will show as a duplicate and only one camera will actually capure clips going forward.
You should still be able to delete the camera after re-adding the appliance as you will see one communicating and one not communicating. Delete the non-communicating camera.
Publié pour:Schneider Electric Algeria