{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
DCE 7.9.3 Communications to an SNMP version 3 device may fail if new passphrases are used.
Issue:
Communications to an SNMP version 3 device in DCE 7.9.3 may fail if new passphrases are used.

Product Line:
Data Center Expert (DCE)

Environment:
Data Center Expert 7.9.3
Potentially any SNMP version 3 device.

Cause:
If you change the SNMP version 3 passphrases for an SNMP version 3 device that is already discovered in DCE, even if you change the SNMP parameters in DCE, you may lose communications and not regain it.

Similarly, if you discover and delete a device, then try to discover with changed SNMP parameters, the device may not properly discover or communicate.

Resolution:
It has been seen that the SNMP parameters are being held in the SNMP daemon and a reboot of the DCE system will clear the old parameters out.

If you have changed passphrases on a device and lost communications within DCE even after updating the passphrases there to, a simple reboot of the DCE server should resolve the communications issue.

This issue should be resolved in an up coming revision of Data Center Expert

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :