{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
How to disable weak ciphers in KVM2132P, KVM2116P, and KVM1116P?
Product Line: KVM2132P, KVM2116P, and KVM1116P

Environment: KVM Switches

Cause: Weak ciphers in KVM switches.

Resolution:
1. Log in to the KVM's web management console and go to Maintenance->Terminal.
KVM-terminal
2. On the terminal window, issue the following commands to disable the weak ciphers:
enabletlsv1.0 0
enabletlsv1.1 0
enablerc4 0
setsslcipher 2

KVM-terminal-tls

KVM-terminal-rc4
3. Each command should provide an output confirming if it is successfully carried out. Issuing the 'get' command shows which ciphers are used by the KVM along with the other statuses.
Here is the description of the commands used:
  • enabletlsv1.0 0 - Disables TLS 1.0
  • enabletlsv1.1 0 - Disables TLS 1.1
  • enablerc4 0 - Disables RC4
  • setsslcipher 2 - Disables DES, 3DES, and sets the cipher strength.

Schneider Electric Algeria

En savoir plus
Produit :
En savoir plus
Produit :