{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Static IP configuration from the serial console appears to not persist after a reboot if a network is not connected.
Issue:
Static IP configuration from the serial console appears to not persist after a reboot if a network is not connected.

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755

Cause:
If you do not have a network cable attached to the NetBotz 750 or 755 and you serially provide it an IP and subsequently reboot the unit, the unit will appear to have no IP set to the public LAN.

Resolution:
Simply connect the appliance to the network and the IP configuration should reappear as configured. It is not lost, it is simply not shown when no network is connected.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :