{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Back-UPS users want a quick and convenient access method to the PowerChute Web UI without the requirement of a username and password.

Issue:
Back-UPS users want a quick and convenient way to access the PowerChute Web UI without requiring a username and password.

Product Line & Device Model:
PowerChute Serial Shutdown
Supported Back-UPS models

Environment:
All supported OS connected to a Back-UPS
Cause:
Informational

Solution:
PowerChute Serial Shutdown v1.2 and above supports Back-UPS users instantly accessing the Web UI via the quick access icon without a username and password combination. This feature benefits users who do not require authenticated or remote access to the Web UI. To enable the quick access feature, deselect "Create a user account". This will allow only a local user to access the PowerChute web interface and no credentials will be required.

Create a user account

NOTE: This feature is only available when connected to a Back-UPS.

Once the installation has completed there will be a PowerChute icon on the desktop and an icon in the Systray.

Quick connect Icon

NOTE: It is recommended that a PowerChute user account be created when the system is on a company or public network.

Existing PowerChute v1.0 users can also remove the username and password requirement by updating to the latest version.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :