Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
		
En quoi pouvons-nous vous aider aujourd'hui ?
Self-test fails on Back-UPS when the test is run from PowerChute Serial Shutdown
Issue:
When running a self-test from PowerChute Serial Shutdown connected to a Back-UPS, the software reported that the self-test had failed.

Products:
Back-UPS BE450G, BE550G, BE550MC, BE650G, BC650-RS, BE700KR, BN700MC
PowerChute Serial Shutdown versions 1.0 and 1.2

Environment:
All supported Windows OS

Cause:
The Back-UPS firmware does not allow a self-test to be run via the software.

Solution:
Run the test manually via the UPS.
To run a self-test, press and hold the power button. You will hear a beep. Continue to hold the button in, and within a few seconds, the power button will begin to flash, indicating the UPS is running a self-test. When the button starts to flash, it can be released.

NOTE: When running a self-test manually as listed above PowerChute may not record the test has been run. This issue will be address in a future release. See Schneider Electric FAQ000267910 PowerChute Serial Shutdown does not report a self-test has run when connected to a Back-UPS.

Schneider Electric Algeria

En savoir plus
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.