{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Troubleshooting "Application is incompatible with this AOS" messages on a Network Management Card
Issue:
When logging into the web interface of a Network Management Card (NMC), the user is presented with an error message that the "Application is incompatible with this APC AOS"

screenshot showing incompatible AOS warning

Product:
All products that use a standalone or embedded NMC, including but not limited to UPS, Rack PDU, and ATS systems.

Environment:
All firmware and serial ranges

Solution:
An incompatible AOS error message can be caused by a number of factors, including but not limited to:
  • An incorrect application image being loaded onto the NMC
  • A failed or partial firmware upgrade
  • Firmware not fully loading on a device
Users may be able to login to the CLI, and could potentially see the following for NMC status:

screenshot showing P N A status of an NMC

Where "A!" means there is an issue with the firmware application on the NMC. To resolve this, users should first try and reflash with the latest firmware version they have access to. If that does not resolve the problem, the next step would be to format the NMC by holding down the NMC pin reset button for 30 seconds (this will wipe all configuration from the card), and if the card is still inaccessible or unable to be given an IP address then upgrade the NMC using the "bootmonitor" method outlined in this article: Video: Using Network Management Card 2 (NMC2) bootmonitor to recover/upgrade firmware

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :