{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Do NetShelter™ Zero U Rack PDUs comes with vertical mounting brackets?
Issue:
Customers are asking if NetShelter™ Zero U Rack PDUs comes with vertical mounting brackets

Product Line:
NetShelter™ Zero U Rack PDUs

Environment:
NetShelter™ Rack PDU Advanced
NetShelter™ Metered Rack PDUs
NetShelter™ Switched Metered Outlet PDUs
NetShelter™ Switched Rack PDUs
NetShelter™ Metered-by-Outlet Rack PDUs

Solution:
NetShelter™ Zero U Rack PDUs do not come with vertical mounting brackets. They can be installed to the vertical accessory channel of a NetShelter™ rack using the included or pre-installed mounting pegs. The pegs will work in most rack enclosure designs. Please refer to the Installation Guide of your NetShelter™ Rack PDU for more info.
PDU Mounting PegsAPDU10K
For 3rd party cabinets, an alternative is utilizing the AR7711 (NetShelter Zero U Accessory Mounting Bracket).
AR7711

Kindly take note that this is specifically designed for NetShelter™ cabinets. We cannot guarantee fitment to 3rd party cabinets. It would be best to get in touch with the 3rd party manufacturer for options or compatibility concerns.

Should there be any further concerns, please contact our Customer Care Center at https://www.apc.com/us/en/support/

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :