{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you use an ATS48 soft starter for a resistive load?
Issue:
Can an Altistart ATS48 soft start be used for a resistive load?

Product Line:
ATS48

Environment:
Resistive Load

Cause:
n/a

Resolution:
No. The ATS48 soft starters can not be used with resistive loads. They require a lagging power factor. Soft starters are designed for motor loads only.

Schneider Electric Egypt and North East Africa