{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How can you identify the coil voltage for the LC2D2501 contactor that was supplied with an ATV66 enclosed package?

Article available in these languages: Spanish

Issue:
What is the coil voltage in an LC2D contactor inside an enclosed drive package?

Product Line:
Tesys D line contactors and Soft starters

Environment:
Products sold and used in the United States

Cause:
Identifying control voltage

Resolution:
Without having specifics on the enclosure part number, look at the A1 and A2 terminations on top of the coil and it will have the control voltage, such as 120v, stamped on it along with the code, such as G6, for the associated voltage.


Schneider Electric Egypt and North East Africa