{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATS48 come with the shorting contactor as a standard component when it is ordered?
Issue:
Wondering if the ATS48 comes with the shorting contactor, as a standard component when it is ordered?

Product Line:
ATS48

Environment:
Shorting contactor

Cause:
n/a

Resolution:
No. It can be ordered as a separate component to be added in the field.

Schneider Electric Egypt and North East Africa