{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the memory for the altivar drive settings and parameters, in the drive, or in the keypad?
Issue:
Settings and parameters saved in the drive or keypad.

Product Line:
Altivar 58

Environment:
All

Cause:
N/A

Resolution:
The actual program that the drive uses to run is stored in the drive control board itself. Removal of the keypad will not alter that program.
NOTE: There is storage memory available in the keypad that can be used to save a copy of the parameter settings. This may not be the same as the actual program that the drive is using.

Schneider Electric Egypt and North East Africa