{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is a replacement contact carrier for a 8502SA or 8536SA controller?
Issue:
Replacement parts for 8502SA or 8536SA Series B

Product Line:
8502/8536 Type S Full Voltage Contactors and Starters

Environment:
Type SA Type SB Type SC, Size 00 Size 0 Size 1

Resolution:
31127-014-01 is the contact carrier only for NEMA size 00, 0 and 1.
This also applies to 8502SB, 8536SB, 8502SC and 8536SC devices.

Contact Carrier

Schneider Electric Egypt and North East Africa