Issue:
NEMA Rating of the XACA Pendant Station
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony XAC Medium-Duty Pendant Stations
Resolution:
It is rated NEMA 4, 4X (indoor and outdoor), and IP65.
Pistol grip NEMA 4, 4X (indoor), and IP65.
NEMA Rating of the XACA Pendant Station
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony XAC Medium-Duty Pendant Stations
Resolution:
It is rated NEMA 4, 4X (indoor and outdoor), and IP65.
Pistol grip NEMA 4, 4X (indoor), and IP65.
Released for:Schneider Electric Egypt and North East Africa