Issue:
Set display to show specific parameters as the default the ATS48.
Product Line:
Altistart 48
Environment:
All
Cause:
Display customization
Resolution:
The factory setting displays the motor current (parameter LCr).
To save the chosen display:
You must make these changes from the keypad on the face of the starter itself. These changes can not be made via the remote keypad, if present.
- Press the ENT key once: the choice is temporary, it will be cleared at the next power up.
- Press the ENT key again for 2 seconds: the display flashes, the choice is permanent and will be retained even if power is cycled.
The available display parameters are:
COS - power factor
LCr - Line current
rnt - hours of run time
LPr - Line power in terms of percentage nominal
Ltr - motor torque in terms of percentage nominal
LAP - Power in terms of kW
EtA - Soft Starter status (rdy, acc, dec, run etc.)
LFt - Last fault detected
PHF - Phase rotation
COd - keypad locking code
Set display to show specific parameters as the default the ATS48.
Product Line:
Altistart 48
Environment:
All
Cause:
Display customization
Resolution:
The factory setting displays the motor current (parameter LCr).
To save the chosen display:
You must make these changes from the keypad on the face of the starter itself. These changes can not be made via the remote keypad, if present.
- Press the ENT key once: the choice is temporary, it will be cleared at the next power up.
- Press the ENT key again for 2 seconds: the display flashes, the choice is permanent and will be retained even if power is cycled.
The available display parameters are:
COS - power factor
LCr - Line current
rnt - hours of run time
LPr - Line power in terms of percentage nominal
Ltr - motor torque in terms of percentage nominal
LAP - Power in terms of kW
EtA - Soft Starter status (rdy, acc, dec, run etc.)
LFt - Last fault detected
PHF - Phase rotation
COd - keypad locking code
Released for: Schneider Electric Egypt and North East Africa