{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATS48 have a automatic restart feature?

Article available in these languages: Spanish

Issue:
Looking for the ATS48 automatic restart feature.

Product Line:
ATS48

Environment:
Auto Restart

Cause:
n/a
Resolution:
Yes, the parameter (ArS)  is located in the PrO menu.
If this function is active and the soft starter locks on a fault, the soft starter automatically restarts if the fault has disappeared and the other operating conditions permit the restart. A series of automatic attempts are made to restart the soft starter at intervals of 60 s. If a restart has not been possible after 6 attempts, the procedure is abandoned and the soft starter remains locked until it is switched off then switched on again or reset manually

The following faults permit this function: PHF, FrF, CLF, USF.
The soft starter fault relay remains activated if this function is active. The run command must be maintained.
This function can only be used in 2-wire control.


Schneider Electric Egypt and North East Africa