{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What will cause an ATV312 ready light to flash and the drive not to run even though speed reference and direction is present?
Issue:
What will cause an ATV312 ready light to flash and the drive not to run even though speed reference and direction is present?

Product Line:
ATV312

Environment:
All

Cause:
Flashing RDY

Resolution:
One possible cause would be if the COS code Power Factor in drC menu is set to 1.0.
Need remove the run command, go to the drC menu, reduce the COS value to the PF (Power Factor) on the motor nameplate, or if you don't see that reduce to .82, then try again to issue a run command.

Schneider Electric Egypt and North East Africa