Search FAQs
Where are the Control Coil Terminals for TeSys D Line Contactors?
Issue:
Control coil terminal marking and location on Tesys D Line contactors
Product Line:
Contactors and Starters-IEC
Environment:
TeSys D Contactors
Resolution:
The coil terminals are marked A1 and A2, you can see them on the front of the contactor. They are next to the auxiliary contact (13/14 NO, 21/22 NC) terminals.
For DC Coils, positive and negative terminals are marked. A1 for positive, A2 for negative.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Range:
Explore more
Product:
Range: