{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is an Analog Output standard on the ATS48 unit?
Issue:
Analog Output on the ATS48 unit.

Product Line:
Altistart 48

Environment:
All

Cause:
Need details on analog output

Resolution:
Yes.
It is a programmable analog output.
Output can be configured as 0-20 mA or 4-20 mA
*Accuracy +/- 5% of the maximum value, maximum impedance 500 ohms

Schneider Electric Egypt and North East Africa