{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for Devicenet Option on ATS48 Softstarter?
Issue:
Is Devicenet option available on ATS48 Softstarter?

Product Line:
ATS48, Altistart 48

Environment:
All

Cause:
NA

Resolution:
There is no Devicenet option card for ATS48. The built-in Communication option is Modbus.
However, part number LUFP9 Gateway is available.
The LUFP9 does require set up as it is not specific for the Altistart 48 product.

Schneider Electric Egypt and North East Africa