{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for Hand-Off-Auto (HOA) Insta-Kit for the LE1D and LE2D metallic enclosed Tesys D-Line contactors or starters?
Issue:
Hand Off Auto kit needed for an enclosed LE*D, IEC starter

Product Line:
IEC Contactors and Starters

Environment:
LE1D Instakit IEC enclosed starters

Cause:
Hand off auto is required in the application

Resolution:
LA9CA06ET is the part number for the Hand-Off-Auto (HOA) selector switch Insta-Kits. This is for field installation.

Schneider Electric Egypt and North East Africa