{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there an LED bulb available for use in XB4 or XB5 with Direct Supply Light Modules?

Issue:
LED Bulbs with BA9s Base

Product Line:
22mm Push Buttons

Environment:
XB4/XB5 Harmony 22mm Push Buttons

Cause:
Spare parts

Resolution:
We only offer green, red and yellow BA9s LED bulbs in 48Vac/dc.
24VAC/DC48VAC/DC6 V - 1.2 W
WhiteDL1CJ0241DL1CD0061
GreenDL1CJ0243DL1CJ0483DL1CD0063
RedDL1CJ0244DL1CJ0484DL1CD0064
OrangeDL1CJ0245DL1CJ0485DL1CD0065
BlueDL1CJ0246DL1CD0066
See attached Digest page for other LED options.

Schneider Electric Egypt and North East Africa

Attachment(s)

Capture.JPG.jpgCapture.JPG.jpg [33.69 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: