Issue:
Clarifying is the closing plates are metal or plastic
Product Line:
9001 30mm
Environment:
North American Products
Resolution:
Both 9001K51 and 9001K52 are plastic. They do come with a metal ring nut that secures the closing plate to the back of the enclosure.
Meets UL and Nema 1, 2, 3, 4, 4x, 6, 12, and 13.
Clarifying is the closing plates are metal or plastic
Product Line:
9001 30mm
Environment:
North American Products
Resolution:
Both 9001K51 and 9001K52 are plastic. They do come with a metal ring nut that secures the closing plate to the back of the enclosure.
Meets UL and Nema 1, 2, 3, 4, 4x, 6, 12, and 13.
Released for:Schneider Electric Egypt and North East Africa