{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the lug torque requirement for the 8910DPA43?

Issue:
8910DP/DPA wire torque

Product Line:
Class 8910 Type DP and Type DPA, Definite Purpose Contactors

Environment:
Series C, Types DP and DPA

Resolution:
Power Terminals
Class 8910 DP = #10-32 screws - 22 inch lb.  Box lugs - 40 inch lb
Class 8910DPA (20A to 40A) =  #10-32 screws - 22 inch lb.  Box lugs - 40 inch lb

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: