Issue:
Part number required for remote mounting the ATV61/71 with the VW3A1101 keypad.
Product Line:
VW3A1101 keypad for ATV61 ATV71 drives
Environment:
All
Cause:
Installation
Resolution:
The mounting kit, including bezel and hardware is VW3A1102
The Modbus cables to connect the keypad to the control basket of the drive are:
5 Meters - VW3A1104R50
10 Meters - VW3A1104R100
The clear plastic door (IP 65 rating) to cover the keypad when not in use is VW3A1103
Part number required for remote mounting the ATV61/71 with the VW3A1101 keypad.
Product Line:
VW3A1101 keypad for ATV61 ATV71 drives
Environment:
All
Cause:
Installation
Resolution:
The mounting kit, including bezel and hardware is VW3A1102
The Modbus cables to connect the keypad to the control basket of the drive are:
1 Meter - VW3A1104R10
3 Meters - VW3A1104R305 Meters - VW3A1104R50
10 Meters - VW3A1104R100
The clear plastic door (IP 65 rating) to cover the keypad when not in use is VW3A1103