Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the size of cable that can be used for the remote connection of time delayed UVR/MN module of Masterpact ACBs.
With the increase in length there always occurs a voltage drop in the cable. Refer the attachment for voltage drop values, according to cable sizes and nominal current.
So you have to consider the size and length of the cable as per the values and load consumption of UVR/MN module.
Standard recommendation is that the voltage supplied to UVR/MN should not be less than 5% of rated voltage, even if the MN can operate down to 0.85Un.
Example:
Time Delay UVR/MN module of 230V AC and Cable size 2.5 sq. mm considered for this example.
Nominal current is pick-up current that is 200VA/230V = 0.9A.
With 2.5sq. mm/1A, voltage drop is 0.8% for 100 meter (as per table attached). This means that one can go up to 625 meter without any problems.
It could be more but keep in mind that minimum supply voltage cannot be less than 0.85Un.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: