Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to deactivate the Earth Fault protection in Micrologic 6.0 trip unit of Masterpact ACB.
To deactivate the Earth Fault protection function in Micrologic 6.0 trip unit, follow the below procedure:
1. On the Masterpact Air Circuit Breaker (ACB), you have to put the jumpers in between F1-M1 and M2-M3 terminals.
2. Remove the External Sensor from the busbars and disconnect the wiring between Sensor and the ACB.
In case External sensor can't be removed from the busbars then remove the wires between Sensor and ACB. Next jumper the sensor terminals T1-T2 and T3-T4.
Refer the attached document describing the procedure.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: