Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the material composition of the Main Bus Bar of the Masterpact ACB?
The material composition used in the Main Bus Bar of the Masterpact Air Circuit breaker (ACB) is shown in the table attached.
Note:
AL/Sn5 means Aluminum connector with Sn5 coated
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: