This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
In Altivar 71 drive from frame Size 2 to 5b the fan starts on a temperature Threshold (THD) = 70%.
And from frame Size 6 to 15 the drive cooling fan starts as soon as the run command is given.
Refer the attachment for the KW details of Altivar 71 Size 2 to 5b and Size 6 to 15.
Released for:Schneider Electric Egypt and North East Africa