{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the braking transistor inbuilt in Altivar 71 Drives?

The Braking transistor is inbuilt in maximum ratings of Altivar 71 Drive.

The following Altivar 71 Drive ranges ATV71HpppM3, ATV71HpppM3X, ATV71H075N4…HC16N4, ATV71WpppN4, ATV71PpppN4Z and ATV71HU22Y…HC16Y have a built-in dynamic brake transistor.
However for the following Altivar 71 Drive ranges ATV71HC20N4…HC50N4 and ATV71HC20Y…HC63Y a braking unit must be used. This is controlled by the Drive.
Refer attachment for the Braking Unit Part reference details.

Schneider Electric Egypt and North East Africa

Attachment(s)
Braking Unit Part Reference.pdf [39.64 KB]