Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Temperature Threshold at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled?
The Temperature Thresholds at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled are as follows:
1. Start – Heatsink Temperature > 50°C.
2. Stop – Heatsink Temperature < 40°C.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: