{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How do you unlock the access of all Drive Parameters in an Altivar 31 Drive

In order to gain access to all the Altivar 31 Drive parameters one of the two conditions will apply:

1. Parameter Access Via Standard Keypad (Integrated LED Display):

Enter the Customer password in parameter Terminal Locking Code (Cod) in Monitoring Menu (Sup).

2. Parameter Access Via Remote Keypad:
a. Enter the Customer password in parameter Terminal Locking Code (Cod) in Monitoring Menu (Sup).
AND
b. Set the Dip Switch called ‘Access Locking Switch’ at the rear portion of the Remote Keypad to ‘Unlock’ position. Refer to the attachment.
Note:
Customer password protection has priority over the switch setting.
Note:
In case the Customer set password is forgotten use the Master password ‘6969’ which resets the customer password and opens access to all parameters.

Schneider Electric Egypt and North East Africa

Attachment(s)
1.jpg [23.9 KB]