{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between a trigger action push-pull or turn to release verses a non-trigger action?
Issue:
Difference between a trigger action mushroom head Emergency-stop push-pull or turn to release operator against a standard non-trigger action operator.

Product Line:
22mm Push Buttons

Environment:
Harmony 22mm

Cause:
Product Features

Resolution:
A standard operator can be depressed enough to open a normally closed contact without latching into the depressed position (also referred to as teasing the contact).
The trigger action units have a spring loaded mechanism that causes the operator to pull fully into the depressed position after a certain actuation distance confirming the operator has been switched.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.