{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between QMB and QMJ fusible branch units?

Issue:
Product Design Features

Product Line:
QMB QMJ panelboards and switchboards

Resolution:
The QMJ switches are suitable for use with Class J fuses only.

The QMB switches as standard accept a Class H or K fuses for use on systems up to 10 kAIC and Class R fuses with a Class R fuse kit for use on systems up to 200 kAIC. Then many of the QMB switches can be modified to accommodate Class J fuses by moving the load base assembly to a location marked on the enclosure. Also, some of the QMJ switches will be in a smaller footprint enclosure.

Schneider Electric Egypt and North East Africa