{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Main Difference between the Motor Circuit breaker of tpye GV2ME and GV2LE ?
Both ranges are a motor Circuit breaker used for motor protection and the main difference is as follows:
- GV2ME: it is a Thermal - Magnetic Motor CB so it provides the protection of motor against Short circuit and Overload (short and long protection) without the need for external thermal overload relay.
- GV2LE: it is a Magnetic only Motor CB so it provides only short protection (Short circuit protection) and it is a must to use external thermal overload relay for the long protection against overload for the motor.

Schneider Electric Egypt and North East Africa