{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do you set up an ATV12 Drive to run in the reverse direction?

Article available in these languages: Czech, French, Dutch

With the seven segment display showing RDy press the center of the Jog Dial which from  now on will be referred to as ENTER, then press the MODE button until the display shows COnF.

At this point press ENTER and then by rotating the Jog Dial scroll down until the display shows FULL and again press ENTER.  The display should now show CFG, from here again using the Jog Dial scroll down until the display shows FUN and again press ENTER the display will now show rPt, scroll down to rrS and press ENTER.

Here you select the digital input you require to be the signal to send the drive in the reverse direction, if your drive is connected in 2 - wire configuration LI1 is reserved for Forward and any of the other inputs can be assigned to reverse.  Normally it is LI2 which is used as reverse so to select your input scroll down until the display shows the required input i.e. L2H and press ENTER, this means that when LI2 is high the drive will run in the reverse direction.

If the drive is being operated in 3 - wire configuration the possible inputs you can use are limited as LI1 becomes the stop signal and LI2 is now run Forward so in this case you can only assign LI3 or LI4 as Reverse

Front view of ATV12 drive

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: