Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what type of software should i use to communicate to TSX momentum PLC in our power distribution system ,one of the models is "171CCS76000" ?
The latest software used with Momentum processor adapters is "Proworx NxT" version 2.5 or higher. In case the processor involved has an old serial number (i.e was programmed using Concept or Modsoft ), Proworx can automatically convert the program to new Proworx formats.
You can find the method for uploading the program on the processor to the PC in the pdf attached.
Also, find attached a list for the supported operating systems.
As for the cable, you can use ( 110 XCA 282 0* ), where you can replace the * with the length of cable required (1= 1m, 2= 3m, 3= 6m).
This is an RS232 (RJ45 to RJ45 ) connector to connect the processor to the PC for programming and simulation.
You can find the method for uploading the program on the processor to the PC in the pdf attached.
Also, find attached a list for the supported operating systems.
As for the cable, you can use ( 110 XCA 282 0* ), where you can replace the * with the length of cable required (1= 1m, 2= 3m, 3= 6m).
This is an RS232 (RJ45 to RJ45 ) connector to connect the processor to the PC for programming and simulation.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: